2016-01-26 7:47 AM
Hello, this is my first time on this forum.
I was using STM32F030F4 for communication with battery (SMBus). I decided to change it for STM32F030CC, but it seems like my I2C1 is not working properly any more. I used the same pins as before, PA9 and PA10, and the same code, but it seems like I2C1 is stuck in busy state. It happens after this line : I2C_TransferHandling(I2C1, 0x16, 1, I2C_SoftEnd_Mode, I2C_Generate_Start_Write);I will try to enter parts of my code which describes I2C1. BTW I have tried some of the tips about this problem(reseting I2C1 after enabling it's clock, defining GPIOS after I2C1 configuration, Enabling I2C1 before I2C_Init) , but it doesn't seem to work, maybe there is some problem in my configuration.&sharpinclude <stm32f0xx_gpio.h>&sharpinclude <stm32f0xx_rcc.h>&sharpinclude <stm32f0xx_i2c.h>&sharpinclude <stm32f0xx_usart.h>&sharpinclude <stm32f0xx.h>&sharpinclude <stm32f0xx_adc.h>&sharpinclude <stm32f0xx_exti.h>&sharpinclude <stm32f0xx_syscfg.h>&sharpdefine SMBUS_CLK_PIN GPIO_Pin_9&sharpdefine SMBUS_DATA_PIN GPIO_Pin_10unsigned char volt_A;unsigned char volt_B;unsigned char temp_A;unsigned char temp_B;void SMBUS_FLAG_BUSY(){ while (I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY)) ; }void read_SMBus() // this loop is because if the battery gets disconnected while communication is happening MCU hangs forever waiting a message{ while (I2C_GetFlagStatus(I2C1, I2C_FLAG_RXNE) == 0) { i++; if (i == 1000) { i = 0; break; } } i = 0;}void PIN_CONFIGURATION(void) { GPIO_InitTypeDef GPIO_InitStructure; I2C_InitTypeDef I2C_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); RCC_I2CCLKConfig(RCC_I2C1CLK_SYSCLK); /* AF - alternate function */ GPIO_PinAFConfig(GPIOA, SMBUS_DATA_PIN, GPIO_AF_4); GPIO_PinAFConfig(GPIOA, SMBUS_CLK_PIN, GPIO_AF_4); //Configure pins: SCL and SDA ------------------ GPIO_InitStructure.GPIO_Pin = SMBUS_DATA_PIN | SMBUS_CLK_PIN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_Init(GPIOA, &GPIO_InitStructure); // I2C configuration I2C_DeInit(I2C1); I2C_Cmd(I2C1, DISABLE); I2C_InitStructure.I2C_Timing = 0xB0420F13; //B0420F13 vai moshk sit? 0x00901D23 I2C_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Enable;// analogaistroksnu filtrs ieslegts I2C_InitStructure.I2C_DigitalFilter = 0x00; // digitalais troksnu filtrs izslegts I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; // pec tam buus siten I2c uz SMBus modi janomaina I2C_InitStructure.I2C_OwnAddress1 = 0x40;// kaa tiek izveeleeta adrese I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; // sitam jaabut bus ieslegtam ari tad kad SMBus buus laikam I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_Cmd(I2C1, ENABLE); I2C_Init(I2C1, &I2C_InitStructure); I2C_TimeoutAConfig(I2C1, 0x63);// I2C_TimeoutBConfig(I2C1, 0x1F); // replacable with I2C1->TIMEOUTR |= 0x801F9063; i guess}int main(void){ PIN_CONFIGURATION(); while(1) { SMBUS_FLAG_BUSY(); I2C_TransferHandling(I2C1, 0x16, 1, I2C_SoftEnd_Mode, I2C_Generate_Start_Write); // now I2C1 is busy I2C_SendData(I2C1, 0x9); I2C_ExtendedClockTimeoutCmd(I2C1, ENABLE); SMBUS_FLAG_BUSY(); I2C_TransferHandling(I2C1, 0x16, 2, I2C_SoftEnd_Mode, I2C_Generate_Start_Read); I2C_SlaveByteControlCmd(I2C1, ENABLE);// In order to allow byte ACK control in slave reception mode, Slave Byte Control mode must be enabled by setting the SBC bit in the I2C_CR1 register. This is required to be compliant with SMBus standards. read_SMBus(); volt_A = I2C_ReceiveData(I2C1); read_SMBus(); volt_B = I2C_ReceiveData(I2C1); SMBUS_FLAG_BUSY(); I2C_TransferHandling(I2C1, 0x16, 1, I2C_SoftEnd_Mode, I2C_Generate_Start_Write); I2C_SendData(I2C1, 0x8); I2C_ExtendedClockTimeoutCmd(I2C1, ENABLE); SMBUS_FLAG_BUSY(); I2C_TransferHandling(I2C1, 0x16, 2, I2C_SoftEnd_Mode, I2C_Generate_Start_Read); I2C_SlaveByteControlCmd(I2C1, ENABLE);// In order to allow byte ACK control in slave reception mode, Slave Byte Control mode must be enabled by setting the SBC bit in the I2C_CR1 register. This is required to be compliant with SMBus standards. read_SMBus(); temp_A = I2C_ReceiveData(I2C1); read_SMBus(); temp_B = I2C_ReceiveData(I2C1); }} #stm32f030cc #i2c1-busy2016-01-26 9:43 AM
I solved this problem.
I guess I'm retarded.
Instead of SMBUS_DATA_PIN and SMBUS_CLK_PIN there must be GPIO_PinSource9 and 10. I thought I can use GPIO_Pin_9 and 10 there , but I was wrong.
instead of this:
/* AF - alternate function */GPIO_PinAFConfig(GPIOA, SMBUS_DATA_PIN, GPIO_AF_4);
GPIO_PinAFConfig(GPIOA, SMBUS_CLK_PIN, GPIO_AF_4);
there should be this: GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_4); GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_4);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.