2016-07-21 3:33 AM
Hello,
I want to try to wake up the F030 out of the standby mode. I enabled HAL_PWR_EnableWakeUpPin, then put the chip into low power mode with HAL_PWR_EnterSTANDBYMode. I know that to wake it up i should make a rising edge to it. I made a pushbutton to give a current to it. For an indication i use blinking LED that so i know if anything is moving, but upon standby mode the led lights up and doesn't come blink after i push the button that should wake up the PA0 pin. Can someone give any advice on what maybe I'm doing wrong or some info on where to move? Would be helpfull, thank you. #- #standby #pwr #stm32f0302016-07-21 6:57 AM
Hi sutkus.rokas,
I suggest you to have a look to this example under the STM32F0 cube firmware package:STM32Cube_FW_F0_V1.6.0\Projects\STM32072B_EVAL\Examples\PWR\PWR_STANDBY It shows how to enter the system to STANDBY mode and wake-up from this mode using: external RESET, RTC Alarm A or WKUP pin.-Syrine-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.