2014-11-06 9:37 PM
Hi,
I am trying to some data from STM32FO devboard(Standard board from ST- MB1304) to PC via usart1. I have created the project in Keil. Data is not transmitting from STM32 to PC. First I thought that code is not running. To check that I have added an led blinking program and then checked. The led starts blinking, but no data via usart. Don't know what went wrong. I think there might be the problem with clock configuration...The code is given below.int main()
{
init_usart();
while(1)
{
while (USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET)
{
USART_SendData(USART1, 'X');
}
}
}
void init_usart()
{
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_0);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_0);
/* Configure USART1 pins: Rx and Tx ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1,ENABLE);
} .Any suggestions....
#stm32f0-usart
2014-11-07 1:31 AM
Hi
''I am trying to some data from STM32FO devboard(Standard board from ST- MB1304)'' Quick search did not find the board (MB1304) you are referring to. Are you referring to this one : If so, the USART output levels are not RS232 (+/- 12V). You need to use a level converter (eg MAX232).2014-11-07 1:50 AM
Yes I am using the same board.
2.I am using FTDI converter to connect the board with PC. So I think that will not be an issue.......2014-11-07 2:21 AM
''2.I am using FTDI converter to connect the board with PC. So I think that will not be an issue.......''
What do you mean 'FTDI converter' ? Pre-assembled converter boards usually convert RS232 (level ie +-12V) to USB from what I know of them. A bare FTDI device (chip) will take logic (5V or 3V) levels. Have you checked with a scope if anything is coming out of GPIO_A IO 9 and 10 ?2014-11-07 2:34 AM
As far as I know, I can connect the said Rx and Tx of ftdi converter to corresponding Tx and Rx pins of the controller and watch the output in serial terminal. (I m doing the same with F1 discovery board also)
I have not checked the output with scope. Do you have any suggestions in the clock configuration part???2014-11-07 2:44 AM
''Do you have any suggestions in the clock configuration part???''
The only thing that looks different from the code I here which works is ''GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_0);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_0); ''
Check that 'GPIO_AF_0' selects the correct alternate function.
2015-06-20 10:57 AM
change as shown inside while loop
USART_SendData(USART1, 'X');while (USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET) { }
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.