2019-06-27 2:38 AM
Hi,
I am using STM32F051 controller. I have done UART initialization coding but I am not getting interrupt for it. Is there any problem with alternate function register configuration. I am using Pin PB6 and PB7 for Uart. Also I tried finding example code for UART interrupt but didn't code for UART (STM32F051). Kindly help.
void UART_config(void){
//-----Enable USART Clock----------------------------------------
RCC->APB2ENR |= RCC_APB2ENR_USART1EN;
// Configure PB6 (Tx) and PB7 (Rx)
GPIOB->AFR[0] |= 0x00000000; //AFRL, PB6, UART1
GPIOB->AFR[0] |= 0x00000000; //AFRL, PB7, UART1
GPIOB->MODER &= ~0x0000F000; //Clear PB6 & PB7
GPIOB->MODER |= GPIO_MODER_MODER6_1; //Alternate Fxn mode
GPIOB->MODER |= GPIO_MODER_MODER7_1; //Alternate Fxn mode
GPIOB->OTYPER &= ~GPIO_OTYPER_OT_6; //Output Push/Pull
GPIOB->OTYPER &= ~GPIO_OTYPER_OT_7; //Output Push/Pull
GPIOB->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR6_1; //PB6 high speed
GPIOB->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR7_1; //PB7 high speed
GPIOB->PUPDR |= GPIO_PUPDR_PUPDR6_0; //PB6 Pull up
GPIOB->PUPDR |= GPIO_PUPDR_PUPDR7_0; //PB7 Pull up
USART1->CR1 = 0x00000000;
USART1->BRR = (SystemCoreClock / 9600);
USART1->CR2 = 0x00000000; //To make number of stop bits 1
USART1->CR1 |=USART_CR1_TE | USART_CR1_UE | USART_CR1_RE | USART_CR1_RXNEIE | USART_CR1_TCIE;
}
void USART1_IRQHAndler(void){
if (USART1->ISR & USART_ISR_RXNE) { // read interrupt
//for read operation
}
if (USART1->ISR & USART_ISR_TXE) {
//for transmit
}
}
2019-06-27 9:46 PM
Make sure the GPIOB clock is enabled before you start writing to its registers.
Note, that USART1TX/RX at PB6 and PB7 is AF0 !!!
The ISR name must match that in the interrupt vectors (startup file), case sensitive:
void USART1_IRQHandler(void) {
You need to enable the interrupt also in NVIC.
NVIC_EnableIRQ(USART1_IRQn);
JW
2019-06-27 10:13 PM
GPIOB clock is enabled, ISR name is also changed and NVIC_EnableIRQ(USART1_IRQn); is done still facing the same problem. Its not going to interrupt. What could be the problem ?
void UART_config(void){
RCC->APB2ENR |= RCC_APB2ENR_USART1EN;
RCC->AHBENR |= RCC_AHBENR_GPIOBEN;
GPIOB->MODER &= ~0x0000F000; //Clear PB6 & PB7
GPIOB->MODER |= GPIO_MODER_MODER6_1; //Alternate Fxn mode
GPIOB->MODER |= GPIO_MODER_MODER7_1; //Alternate Fxn mode
GPIOB->AFR[0] = 0x00000000; //AFRL, PB6, UART1
GPIOB->AFR[0] = 0x00000000; //AFRL, PB7, UART1
GPIOB->OTYPER &= ~GPIO_OTYPER_OT_6; //Output Push/Pull
GPIOB->OTYPER &= ~GPIO_OTYPER_OT_7; //Output Push/Pull
GPIOB->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR6_1; //PB6 high speed
GPIOB->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR7_1; //PB7 high speed
GPIOB->PUPDR |= GPIO_PUPDR_PUPDR6_0; //PB6 Pull up
GPIOB->PUPDR |= GPIO_PUPDR_PUPDR7_0; //PB7 Pull up
USART1->CR1 = 0x00000000;
USART1->BRR = (SystemCoreClock / 9600);
USART1->CR2 = 0x00000000; //To make number of stop bits 1
USART1->CR1 |= USART_CR1_UE | USART_CR1_RE | USART_CR1_RXNEIE | USART_CR1_TE;
NVIC_EnableIRQ(USART1_IRQn);
}
void USART1_IRQHandler(void){
if (USART1->ISR & USART_ISR_RXNE) { // receive
}
if (USART1->ISR & USART_ISR_TXE) { //transmit
}
}
2019-06-27 10:26 PM
Perhaps it is not actually receiving anything?
Check if any Error/Status flagging.
Check if viable in a polled mode.
Try having it service TXE by sending an 0x55 character, and scope that for bit timing verification.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.