2016-08-02 12:25 PM
Hi ,
I interested in measuring STM32F0 temperature and reference voltage using internal sensor of it's processor at the same time using UART. so I used channels like this;ADC_ChannelConfig(ADC1, ADC_Channel_16 , ADC_SampleTime_55_5Cycles); ADC_TempSensorCmd(ENABLE);ADC_ChannelConfig(ADC1, ADC_Channel_Vrefint , ADC_SampleTime_55_5Cycles);ADC_VrefintCmd(ENABLE);Now I can measured only one values properly..If I applied to read two channel at the same time.I mixed volues eachother. I also looked for multichannel adc titles in the forum but it didn't work properly again. I think should use dma but I'm not good now.Thank you in advance for your help.Regards.2016-08-22 8:13 AM
Hi felisleo,
I suggest you have a look to the 2 following examples available in the package:- STM32Cube_FW_F0_V1.6.0\Projects\STM32F072RB-Nucleo\Examples_LL\ADC\ADC_MultiChannelSingleConversion- STM32Cube_FW_F0_V1.6.0\Projects\STM32F072RB-Nucleo\Examples\ADC\ADC_SequencerIn both examples, the two internal channels (temperature sensor and VrefInt) are converted.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-08-22 11:41 AM
If you have two channels DMAing into an array in continuous/circular fashion you shouldn't get them mixed up. So I'm assuming you're trying to poll them.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.