2015-10-29 7:02 AM
What is wrong here?
I try to read 2 bytes data of temperature sensor LM73 by I2C of STM32F0Discovery based on STM32F051 micro. The micro is waiting RXNE event and doesn't exit from the loop.I don't see any activity on SDA and SCL lines The signals have the pullup resistors.Here is a code bellow:void init_I2C1(void) {
I2C_InitTypeDef I2C1_InitStructure; // I2C1 Configuration structure /** I2C1 GPIO Configuration PB6 ------> I2C1_SCL PB7 ------> I2C1_SDA */ /*Enable or disable the AHB peripheral clock */ RCC_I2CCLKConfig(RCC_I2C1CLK_HSI); RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); /* IC1 Configuration */ // I2C_Cmd(I2C1,DISABLE); /*Configure GPIO pin : PB */ GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6|GPIO_Pin_7; GPIO_InitStruct.GPIO_OType = GPIO_OType_OD; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOB, &GPIO_InitStruct); I2C1_InitStructure.I2C_Mode = I2C_Mode_I2C; /*Timing register value is computed with the AN4235 xls file, fast Mode @400kHz with I2CCLK = 48MHz, rise time = 140ns, fall time = 40ns */ I2C1_InitStructure.I2C_Timing = 0x00B01A4B;// 400KHz | 8MHz-0x00310309; 16MHz-0x10320309; 48MHz-50330309 I2C1_InitStructure.I2C_OwnAddress1 =0; I2C1_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C1_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Enable; I2C1_InitStructure.I2C_DigitalFilter = 0x00; I2C1_InitStructure.I2C_OwnAddress1 = 0x00; I2C1_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C1_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_Init(I2C1, &I2C1_InitStructure); I2C_MasterRequestConfig(I2C1,I2C_Direction_Receiver); // Master reading mode I2C1->CR1 |= I2C_IT_RXI; // Enable RXNE Event// GPIO_SetBits(GPIOB,GPIO_Pin_8);// Power up Delay(10); I2C_Cmd(I2C1,ENABLE);/*Read function*/void I2C1MasterBufferRead() {I2C_TransferHandling(I2C1,(LM73_BASE_ADDR),2,I2C_AutoEnd_Mode,I2C_Generate_Start_Read);
while(I2C_GetFlagStatus(I2C1, I2C_FLAG_RXNE) == RESET); ucI2CReadBuff[0] = I2C_ReceiveData(I2C1); while(I2C_GetFlagStatus(I2C1, I2C_FLAG_RXNE) == RESET); ucI2CReadBuff[1] = I2C_ReceiveData(I2C1); while(I2C_GetFlagStatus(I2C1, I2C_ISR_STOPF) == SET); I2C_ClearFlag(I2C1,I2C_FLAG_STOPF); }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.