2017-06-29 7:40 PM
F0 cube library's SPI API has problems.
In spite of running 8 bit transmission mode, the library transmit a 16 bit data.
So the misalignment check routine does not filter the unaligned address on 8 bit mode.
Then, I think this 8 bit transmission code does not communicate with 16 bit transmission,
the way F4 cube library works.
It's not welcome method, because user can not expect inside 16 bit transmission of the SPI API functions.
2017-07-03 7:43 AM
Hi
Whang.Se_Hee
,I think your are using an old STM32CubeF0 version, asthis limitation is fixed within the STM32CubeF0 firmware package V1.8.0 (available since 07-April-2017)
Regards
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.