2018-03-21 7:14 AM
Latest version gives me this when I want to create a new project
2018-03-21 15:13:32,765 [INFO] About:226 - Version : DB.4.0.2502018-03-21 15:13:35,366 [INFO] McuFinderGlobals:23 - Set standalone mode to false2018-03-21 15:13:35,763 [INFO] LoadUrlFilesThread:141 - End of LoadServerUrlFiles without ThreadException in thread 'AWT-EventQueue-0' java.lang.NullPointerException at com.st.microxplorer.mcuselector.CtxGFX.buildToolTipWidget(CtxGFX.java:40) at com.st.microxplorer.mcuselector.CtxGFX.getPopup(CtxGFX.java:36) at com.st.microxplorer.mcuselector.PanelToolTipUI.setToolTip(PanelToolTipUI.java:152) at com.st.microxplorer.mcuselector.GraphicSummaryPanel.setTooltips(GraphicSummaryPanel.java:214) at com.st.microxplorer.mcuselector.GraphicSummaryPanel.<init>(GraphicSummaryPanel.java:84) at com.st.microxplorer.mcuselector.McuMultiScanPanel.createDetailGUI(McuMultiScanPanel.java:170) at com.st.microxplorer.selector.MultiScanPanel.createGUI(MultiScanPanel.java:371) at com.st.microxplorer.mcuselector.McuMultiScanPanel.<init>(McuMultiScanPanel.java:140) at com.st.microxplorer.selector.McuBoardSelectorDialog.defineWindowsFields(McuBoardSelectorDialog.java:386) at com.st.microxplorer.selector.McuBoardSelectorDialog.init(McuBoardSelectorDialog.java:96) at com.st.microxplorer.selector.McuBoardSelectorDialog.<init>(McuBoardSelectorDialog.java:79) at com.st.microxplorer.plugins.filemanager.engine.MainFileManager.userNewConfig(MainFileManager.java:100) at com.st.microxplorer.plugins.filemanager.FileManagerView$1.actionPerformed(FileManagerView.java:397) at javax.swing.AbstractButton.fireActionPerformed(AbstractButton.java:2022) at javax.swing.AbstractButton$Handler.actionPerformed(AbstractButton.java:2348) at javax.swing.DefaultButtonModel.fireActionPerformed(DefaultButtonModel.java:402) at javax.swing.DefaultButtonModel.setPressed(DefaultButtonModel.java:259) at javax.swing.plaf.basic.BasicButtonListener.mouseReleased(BasicButtonListener.java:252) at java.awt.AWTEventMulticaster.mouseReleased(AWTEventMulticaster.java:289) at java.awt.Component.processMouseEvent(Component.java:6533) at javax.swing.JComponent.processMouseEvent(JComponent.java:3324) at java.awt.Component.processEvent(Component.java:6298) at java.awt.Container.processEvent(Container.java:2237) at java.awt.Component.dispatchEventImpl(Component.java:4889) at java.awt.Container.dispatchEventImpl(Container.java:2295) at java.awt.Component.dispatchEvent(Component.java:4711) at java.awt.LightweightDispatcher.retargetMouseEvent(Container.java:4889) at java.awt.LightweightDispatcher.processMouseEvent(Container.java:4526) at java.awt.LightweightDispatcher.dispatchEvent(Container.java:4467) at java.awt.Container.dispatchEventImpl(Container.java:2281) at java.awt.Window.dispatchEventImpl(Window.java:2746) at java.awt.Component.dispatchEvent(Component.java:4711) at java.awt.EventQueue.dispatchEventImpl(EventQueue.java:758) at java.awt.EventQueue.access$500(EventQueue.java:97) at java.awt.EventQueue$3.run(EventQueue.java:709) at java.awt.EventQueue$3.run(EventQueue.java:703) at java.security.AccessController.doPrivileged(Native Method) at java.security.ProtectionDomain$JavaSecurityAccessImpl.doIntersectionPrivilege(ProtectionDomain.java:80) at java.security.ProtectionDomain$JavaSecurityAccessImpl.doIntersectionPrivilege(ProtectionDomain.java:90) at java.awt.EventQueue$4.run(EventQueue.java:731) at java.awt.EventQueue$4.run(EventQueue.java:729) at java.security.AccessController.doPrivileged(Native Method) at java.security.ProtectionDomain$JavaSecurityAccessImpl.doIntersectionPrivilege(ProtectionDomain.java:80) at java.awt.EventQueue.dispatchEvent(EventQueue.java:728) at java.awt.EventDispatchThread.pumpOneEventForFilters(EventDispatchThread.java:201) at java.awt.EventDispatchThread.pumpEventsForFilter(EventDispatchThread.java:116) at java.awt.EventDispatchThread.pumpEventsForHierarchy(EventDispatchThread.java:105) at java.awt.EventDispatchThread.pumpEvents(EventDispatchThread.java:101) at java.awt.EventDispatchThread.pumpEvents(EventDispatchThread.java:93) at java.awt.EventDispatchThread.run(EventDispatchThread.java:82)2018-03-21 10:48 AM
This error is common if using OpenJDK/JRE. Us the Oracle JRE and the issue goes away.
You can use the `alternatives --config java` command and select the Oracle Java as the default.
2018-03-21 2:02 PM
I have Oracle JDK 1.8.0.162-r1 so that cannot be the issue.
2018-03-21 5:05 PM
I am on (K)ubuntu 17.10 and using
openjdk version '1.8.0_151'
OpenJDK Runtime Environment (build 1.8.0_151-8u151-b12-0ubuntu0.17.10.2-b12)OpenJDK 64-Bit Server VM (build 25.151-b12, mixed mode)I have been using 4.25 successfully daily (with previously created projects) and just created a project now without issues.
I'm guessing some other dependency???
2018-05-14 3:38 PM
Only update the software as `root`...otherwise some things are not written to their place even if you have premission on the folders.
I had the same issue, I just reinstalled the latest version using `root` then used the program with my own user account and it worked again!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.