2018-06-16 7:38 PM
Hi,
I think I encountered with code generation error of STM32CubeMX v4.26.0 in Makefile setting. This is how to regenerate it:
1. Create any project
2. Generate code with Makefile setting.
3. Close CubeMX
4. Find the project folder and open up CubeMX by double clicking on the ioc file.
5. Try to regenerate code.
Workaround is to delete Makefile (and Makefile_tmp if exists) before opening up the CubeMX. So it looks like CubeMX failed to overwrite existing Makefile.
Thanks,
2018-06-27 7:09 AM
Hi lee,
This will be fixed soon in the 4.27.0
2018-09-19 11:14 PM
I'm still facing that error in STM32CubeMX 4.27.0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.