2016-05-19 2:09 PM
In linux STM32CubeMX v4.14.0 doesn't allow NVIC priority changing.
Under the Configuration tab / NVIC Settings after enabling an interrupt the Priority and Sub Priority fields are still read-only and fixed at 0,0 so all the generated code has all the interrupts at the same priority.2016-05-20 3:16 AM
Hello Emil,
When freeRTOS is enabled, the priority group is defined with 4 bits for pre-emption and 0 bits for sub-priority. When freeRTOS is disabled, you can work with sub-priority 15, but in this case you need to change the priority group to be able to choose sub priority > 0.You can refer to this , section (4.12.5 NVIC Configuration window) for more details.Regards2016-05-20 3:30 PM
Let me better exemplify what I've meant: Say you use the SPI1 peripheral, then when you click on the SPI1 button in Configuration under NVIC tab you can enable/disable the interrupt but you cannot change priority and sub-priority although those fields are displayed and I don't think this is the intended behaviour.
Now if you click the NVIC button instead then you have a list of all the enabled interrupts and you can edit there the priorities for all your peripherals.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.