2016-05-17 5:29 AM
I'm a beginner in USB Stack on STM32F4. I have a question about creating a project using CubeMX (STM32F4 Discovery) for USB CDC to have 2 Virtual Com Ports in the ''Device Manager'' ? Thanks
2016-05-19 6:28 AM
Hi,
You should install STM32CubeMx version 4.14.0 from this In CubeMx 'Pinout' tab, you should enable the USB_OTG_FS peripheral as Device Only.Then, in the 'Configuration' tab, enable Midlleware USB_Device with (CDC Virtual Port Com).Make sure to have the STM32 Virtual COM Port Driver on your PC, downloadable at It should then drive the VCP through ST-Link. If your board is connected to the USB, a virtual com port is created and it appears in the windows device manager under ''Ports (COM & LPT)''. PS: About the code generation, you can refer to this CDC application provided within the STM32CubeF4 version 1.11.0 : STM32Cube_FW_F4_V1.11.0\Projects\STM32469I-Discovery\Applications\USB_Host\CDC_StandaloneThis application can help you as an implementation example. RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.