2018-02-22 6:24 AM
Hello,
Have a STM32L432 Nucleo 32 board. I am using the CubeMX to initialise some code and I see in Workbech that within drivers/CMSIS there are much more files that others STM32 projects.
The point is that there two folders: DSP_Lib and Include within CMSIS that are 'in red' because the system can not find the definitions of int8_t, int16_t...etc.
Does anyone the solution for that problem?
Thanks!
2018-02-27 6:10 AM
Hi
Jose.Jose
,It will be helpful if you may share your .ioc file to reproduce issue you have.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-02-28 3:18 PM
Hi,
Something weird is happening. The problematic project is withing a folder with other projects, so when I select the project I see the problem that I mentioned. Today I tried to open directly the folder where the project is and Workbench can not import it because says that the project file is corrupt.
I generated again the project using CubeMX in a different folder and now I can import and compile the project normally.
BTW I was told to try Atollic True Studio and I could import the project without problem as well.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.