2015-05-09 10:41 AM
Hi
All generated file headers are providing date/time in their headers. When doing a re-generate code, some files are re-created exactly the same except the generated date-time. That's really annoying when using version control system which asks you to commit changes while obviously there are not. I can see two solutions for this issue ; - remove the date-time from the file (useless when using vcs but may be usefull...) - compare the new generated ''active code'' of the file and write on the disk only if there are changes. Regards Julien2015-05-11 2:04 AM
Just adding my vote for this feature.
2015-05-12 5:54 AM
+1
2015-05-17 2:26 AM
+1
Really annoying, makes the commits hard to navigate and hides the real changes.2015-05-19 9:08 AM
Hi,
This request is already raised in . It should be implemented in next release (4.8.0). -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.