cancel
Showing results for 
Search instead for 
Did you mean: 

STM3240G-EVAL MCO

jo
Associate II
Posted on March 17, 2015 at 10:01

Is it possible to clock the MCO1 at 50MHz? I have HSE of 25MHz? I did not find instructs.

#stm3240g-eval
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on March 17, 2015 at 13:24

You'd have to run the processor at a multiple of 50 MHz, ie 150 MHz, and divide down from there. You'd want to check if the PLL generates too much jitter/phase-noise for ethernet applications.

The processor will take an external clock source up to 50 MHz via HSE input.

Also there is the I2SPLL via MCO2

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jo
Associate II
Posted on March 27, 2015 at 18:00

@Clive: tnx, it works but it is not the preffered way.

@Jan: :) It sounds like much frustration.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.