2009-08-18 4:04 AM
STM3210E-Eval + blinking test programm from Keil do not work !!!
2011-05-17 4:20 AM
Hi roger,
This example in the default Keil/Uvision installation is for the ''STM3210B-EVAL'' board from ST and not for the board that you have. I highly recommend you to use the latest firmware from our web site if you would like run it on our boards :http://www.st.com/stonline/products/support/micro/files/stm32f10x_stdperiph_lib.zip
. Cheers, STOne-32.2011-05-17 4:20 AM
Here is my technical problems:
1. I've got STM3210E-EVAL evaluation board from ST company. - target STM32F103ZE I've tried to programm it's flash with ULINK-ME USB-JTAG on the base of simple led blinking test programm. (Taken from C:\Keil\ARM\Boards\ST\STM32F10x_Eval\Blinky The flash programming is performing, but I cann't see results - the programm not functions. What can I do ? Is it possible use ULINK-ME USB-JTAG for STM3210E-EVAL board? 2. The flash programming is performing only to use the download button. Normaly I can flash the programm by use the debug button. But in this case it works not. Some details: OS : WINDOWS XP IDE-Version: µVision3 V3.90 Copyright (c) Keil Elektronik GmbH / Keil Software, Inc. 1995 - 2009 License Information: LEV USER COMPANY LIC=---- Tool Version Numbers: Toolchain: RealView MDK-ARM Version: 3.80a Toolchain Path: BIN31\ C Compiler: Armcc.Exe V4.0.0.524 [Evaluation] Assembler: Armasm.Exe V4.0.0.524 [Evaluation] Linker/Locator: ArmLink.Exe V4.0.0.524 [Evaluation] Librarian: ArmAr.Exe V4.0.0.524 [Evaluation] Hex Converter: FromElf.Exe V4.0.0.524 [Evaluation] CPU DLL: SARMCM3.DLL V3.80a Dialog DLL: DARMSTM.DLL V1.43 Target DLL: BIN\UL2CM3.DLL V1.50 Dialog DLL: TARMSTM.DLL V1.43 **************************************************We’re moving the ST Community to a new platform to give you a better and more reliable community experience.