cancel
Showing results for 
Search instead for 
Did you mean: 

STM32103zt6 use with 8-bit Perpherals

sabasit2006
Associate II
Posted on November 05, 2008 at 06:51

STM32103zt6 use with 8-bit Perpherals

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
sabasit2006
Associate II
Posted on May 17, 2011 at 12:49

Dear all,

I am using STM32F10ZET6 microcontroller. I have a query related peripherals interfacing with MCU.

Question:

How do I interface 8-bit peripheral chips like MT8980 (Digital Crosspoint Switch), M34116 (PCM Conference Chip), etc with the STM32F103ZET6 MCU?

In the memory mapping diagram, there are FSMC banks used for memory mapping. Kindly tell me what should I do for the I/O mapping at which address locations?

reply as soon as possible.

regards,

Syed Abdul Basit

Development Engineer

Precision Technology

Cell #: +92-334-3549727

pt1
Associate II
Posted on May 17, 2011 at 12:49

Hi,

it is sometimes easier to talk with external components via direct using the port. You may configure portbits 0-7 for data and portbits 8-15 for handshake: CS, RD~, WR~ ...

Then set and reset the bits by portpin access. This works fine if you don't have to much data to transfer.

Best regards Edi

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.