2010-02-15 6:33 AM
STM32 Virtual COM problem
2011-05-17 4:40 AM
Hi,
Please, which STM32 chip are you using, on which board and which version of the USB Library ?2011-05-17 4:40 AM
Hi,
I made a small test and I got much more than the 400Hz, nearly 1000 Hz (for packets of 60-bytes), and it works fine (please check the snapshot in attachments)... You may have some special conditions over USART/Data ... ?2011-05-17 4:40 AM
Hi there, sorry for the late i'm answering.
I'm using the STM32F10X-128K-EVAL with STM32F103VB and the USB library is STM32_USB-FS-Device_Lib_V3.1.0 I'm planning to run this firmware on a STM32F102R8. Do you think I'm gonna have any problem with that? Thanks2011-05-17 4:40 AM
If you are using STM32F103 I don't think you'll have issues.. all issues posted on forum for v3.1.0 are relative to STM32105/7 devices...
Good luck :)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.