2018-03-08 6:22 AM
I attended the STM8-32 hands on day in Cambridge in Feburary 2018.
I have been repeating or doing the exercises that we did on the day but I have been unable to program the target STM32F072RB nucleo board in three of the four examples. Unfortuately my PC needed to restart on the day then it would not restart so although I had all the programmes and packs installed and had completed the first project but not as far as running ST-link.
I have partly repeated the exercise on another PC unsuccessfully. So it does not apear to be a bad installation issue?
In three of the exercises this is what is reaported after I press debug;
Load 'C:\\Users\\Owner\\Google-Drive\\STM32_Work\\STM32_hands_on_1\\Objects\\STM32_hands_on_1.axf'
No Algorithm found for: 08000000H - 0800038BH Erase skipped! Error: Flash Download failed - 'Cortex-M0' Flash Load finished at 13:28:40I think the pack which is a problem is thjat the Keil .....DFP pack needs to be reloaded every time I create a project but then the target MCU cannot be found;
Keil STM32F072RBxx-DFP
Could not find STM32F072RBTx so selected one of those.Lastly it is the first ST-cube example hands on 1 that is successful but the vartion for HAL fails similarly to the above.
#uvision-evaluation #nucleo-f072rb #stm32-hands-on-day-feb-2018 #failed-pack-stm32f072rbxx-dfpSolved! Go to Solution.
2018-03-09 7:12 AM
Hello Tilen,
Thanks. I needed to highlight STM32F0xx 128kB FLASH as you say in your last sentance for each example. Then the examples all programmed and launched the debugger properly.
Regards
Andrew
2018-03-08 11:05 PM
Hello
Lohmann.Andrew
,if you have installed STM32F0 DFP pack, then there isSTM32F072RB option aswell. Some packages from Keil have different name for MCU option, so please follow theSTM32F072RB and then select closest MCU. If there is an option withTx at the end, use this option.T in this case meansLQFP package.
Regarding flash download algorithm, if you go toOptions for target, thenDebug tab, you chooseST-Link Debugger, thenSettings, underFlash download tab you need your algorithm. If you don't have it in a list, clickAdd to add new and selectSTM32F0xx 128kB FLASH option.
Best regards,
Tilen
2018-03-09 7:12 AM
Hello Tilen,
Thanks. I needed to highlight STM32F0xx 128kB FLASH as you say in your last sentance for each example. Then the examples all programmed and launched the debugger properly.
Regards
Andrew
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.