2010-07-07 2:50 PM
STM32 - uTasker project update
2011-05-17 4:57 AM
Hi mjbcswitzerland,
I have tried to test this tool but when I started filling the ''µTasker license request formular'' I didn't find STM32 port. Only STR9, luminary, AT, AVR and LPC. How could I proceed ? Thanks in advance. Regards, lowpower.2011-05-17 4:57 AM
Hi lowpower
Presently there is only an executable (simulator) and binary demo of the new STM32 project and no developers' package as such. These can be downloaded and tested by anyone at the given link - the project (developers' package) will be made available in the near future but there is still some work involved (like documentation, USB and an IPv4/v6 dual-stack which will be included in the next releases). Note that there are several projects available ranging from Coldfire through AVR32, ARM7, ARM9 and various Cortex M3 parts - the STM32 will become the main ST focus since it is nice chip (in the targeted device class) and the STR91XF project will be phased out (i.e. generally no further active development). If you have real interests in a Beta version for your tests please contact me at the ''info'' address on the uTasker web site because this can certainly be arranged for serious users. Cheers Mark2011-05-17 4:57 AM
Hi All
So that you can get a better idea of the project a video had been added here: I hope that you enjoy it. Regards MarkWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.