2016-01-31 7:51 PM
Hi:
My project use STM32F427compiled at uVision 5.11, I use USB library V2.1.0 for MSC Host class. It builds OK and works OK. Then I try to merge HID host lib, now the compiler report link error L6985E when I add a line to change class callback function from USBH_MSC_cb to HID_cb (These two callback funs are from library example, which can build OK on original example. I can't see the relationship between link errorL6985E and HID host function. The reported address 0x40024000 location is at backup RAM, where I defined as a variable array, seems nothing to do with USB HID class.Here is the link message:
compiling usbh_hid_mouse.c...compiling usbh_usr_lcd.c...linking....\OBJ\st_firmware.axf: Error: L6985E: Unable to automatically place AT section stm32variable.o(.ARM.__AT_0x40024000) with required base address 0x40024000. Please manually place in the scatter file using the --no_autoat option. Not enough information to list image symbols.Finished: 1 information, 0 warning and 1 error messages.''.\OBJ\ut80_st_firmware.axf'' - 1 Error(s), 11 Warning(s). The link error happens when I try to change class callback function depending on MSC or HID device after USB emulation.void USBH_Process(USB_OTG_CORE_HANDLE *pdev , USBH_HOST *phost){ .... switch (phost->gState){ case HOST_IDLE : .... break; case HOST_DEV_ATTACHED : .... break; case HOST_ENUMERATION: /* Check for enumeration status */ if ( USBH_HandleEnum(pdev , phost) == USBH_OK){ /* The function shall return USBH_OK when full enumeration is complete */ /* user callback for end of device basic enumeration */ phost->usr_cb->EnumerationDone(); if(UsbStatus.bi.port_status == USB_DEVICE_STICK){ USBH_SetClass(phost, &USBH_MSC_cb); } else{USBH_SetClass(phost, &HID_cb);
// If remark this line, It builds OK. } phost->gState = HOST_USR_INPUT; } break; .... ....where:void USBH_SetClass(USBH_HOST *phost, USBH_Class_cb_TypeDef *class_cb){ phost->class_cb = class_cb;}And the location for 0x40024000 is defined as: float backup[1024] __attribute__((at(0x40024000 )));The clas callback function is:typedef struct _USBH_Class_cb{ USBH_Status (*Init)\ (USB_OTG_CORE_HANDLE *pdev , void *phost); void (*DeInit)\ (USB_OTG_CORE_HANDLE *pdev , void *phost); USBH_Status (*Requests)\ (USB_OTG_CORE_HANDLE *pdev , void *phost); USBH_Status (*Machine)\ (USB_OTG_CORE_HANDLE *pdev , void *phost); } USBH_Class_cb_TypeDef;USBH_Class_cb_TypeDef USBH_MSC_cb = { USBH_MSC_InterfaceInit, USBH_MSC_InterfaceDeInit, USBH_MSC_ClassRequest, USBH_MSC_Handle,};USBH_Class_cb_TypeDef HID_cb = { USBH_HID_InterfaceInit, USBH_HID_InterfaceDeInit, USBH_HID_ClassRequest, USBH_HID_Handle}; #stm32We’re moving the ST Community to a new platform to give you a better and more reliable community experience.