2020-02-29 12:22 PM
Greetings,
I am dealing with a STM32H743ZI MCU and many of its embedded peripherals, the board is a NUCLEO H743ZI2
I encounter a strange behaviour regarding SPI configuration, for SPI 1 the MOSI pinout works as expected, but for SPI 3 and SPI 4 the MOSI doesn´t work; there are no output from MOSI pin.
I am using the GPIO alternate function configuration from the STM32H742xI/G STM32H743xI/G document (its a 357 pages one), there are several tables that list the corresponding AF for each pin and desired functionality.
The initialization code (for SPI4) I am using is this one (the same for SPI 1 works well, obviously with corresponding GPIO and AF for SPI 1):
/* SPI handler 4 declaration */
SPI_HandleTypeDef SpiHandle4 __attribute__((section(".ramd2")));
void SPI4_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* Chip Select pin is controlled by the SPI4 code */
/* Enable GPIOE clock */
__HAL_RCC_GPIOE_CLK_ENABLE();
/* Configure PE.2 pin as output */
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Pin = GPIO_PIN_2;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* Configure pinout for SCK, MISO y MOSI of SPI4 */
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable GPIO TX/RX clock and SPI4 clock*/
__HAL_RCC_GPIOE_CLK_ENABLE(); /* SCK Port */
__HAL_RCC_GPIOE_CLK_ENABLE(); /* MISO Port */
__HAL_RCC_GPIOE_CLK_ENABLE(); /* MOSI Port */
__HAL_RCC_SPI4_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* SPI SCK GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_2;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI4;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* SPI MISO GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI4;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* SPI MOSI GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_6;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI4;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/*##-1- Configure the SPI4 peripheral #######################################*/
/* Set the SPI4 parameters */
SpiHandle4.Instance = SPI4;
SpiHandle4.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
SpiHandle4.Init.Direction = SPI_DIRECTION_2LINES;
SpiHandle4.Init.DataSize = SPI_DATASIZE_8BIT;
SpiHandle4.Init.FirstBit = SPI_FIRSTBIT_MSB;
SpiHandle4.Init.TIMode = SPI_TIMODE_DISABLE;
SpiHandle4.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
SpiHandle4.Init.CRCPolynomial = 7;
SpiHandle4.Init.CRCLength = SPI_CRC_LENGTH_8BIT;
SpiHandle4.Init.NSS = SPI_NSS_SOFT;
SpiHandle4.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
SpiHandle4.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE;/* Recommended setting to avoid glitches */
SpiHandle4.Init.Mode = SPI_MODE_MASTER;
HAL_SPI_DeInit(&SpiHandle4);
if (HAL_SPI_Init(&SpiHandle4) != HAL_OK) {
/* Initialization Error */
Error_Handler();
}
}
void SPI4_select(void)
{
HAL_GPIO_WritePin(GPIOE, (uint16_t)GPIO_PIN_2, GPIO_PIN_RESET);
}
void SPI4_deselect(void)
{
HAL_GPIO_WritePin(GPIOE, (uint16_t)GPIO_PIN_2, GPIO_PIN_SET);
}Each MOSI pin works as GPIO output if I configure these for this test purpose, in order to check if the pin has any electric problem.
For SPI 3 the initialization code is:
/* SPI handler 3 declaration */
SPI_HandleTypeDef SpiHandle3 __attribute__((section(".ramd2")));
void SPI3_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* Chip Select pin is controlled by the SPI3 code */
/* Enable GPIOE clock */
__HAL_RCC_GPIOE_CLK_ENABLE();
/* Configure PE.2 pin as output */
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Pin = GPIO_PIN_2;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* Configure pinout for SCK, MISO y MOSI of SPI3 */
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable GPIO TX/RX clock and SPI3 clock*/
__HAL_RCC_GPIOC_CLK_ENABLE(); /* SCK Port */
__HAL_RCC_GPIOC_CLK_ENABLE(); /* MISO Port */
__HAL_RCC_GPIOC_CLK_ENABLE(); /* MOSI Port */
__HAL_RCC_SPI3_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* SPI SCK GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* SPI MISO GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_11;
GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* SPI MOSI GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_12;
GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*##-1- Configure the SPI3 peripheral #######################################*/
/* Set the SPI3 parameters */
SpiHandle3.Instance = SPI3;
SpiHandle3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
SpiHandle3.Init.Direction = SPI_DIRECTION_2LINES;
SpiHandle3.Init.DataSize = SPI_DATASIZE_8BIT;
SpiHandle3.Init.FirstBit = SPI_FIRSTBIT_MSB;
SpiHandle3.Init.TIMode = SPI_TIMODE_DISABLE;
SpiHandle3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
SpiHandle3.Init.CRCPolynomial = 7;
SpiHandle3.Init.CRCLength = SPI_CRC_LENGTH_8BIT;
SpiHandle3.Init.NSS = SPI_NSS_SOFT;
SpiHandle3.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
SpiHandle3.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE;/* Recommended setting to avoid glitches */
SpiHandle3.Init.Mode = SPI_MODE_MASTER;
HAL_SPI_DeInit(&SpiHandle3);
if (HAL_SPI_Init(&SpiHandle3) != HAL_OK) {
/* Initialization Error */
Error_Handler();
}
}
void SPI3_select(void)
{
HAL_GPIO_WritePin(GPIOE, (uint16_t)GPIO_PIN_2, GPIO_PIN_RESET);
}
void SPI3_deselect(void)
{
HAL_GPIO_WritePin(GPIOE, (uint16_t)GPIO_PIN_2, GPIO_PIN_SET);
}Do you now what is the reason of non working MOSI pin?
Thanks for yout support mates,
2020-03-01 1:42 AM
SCK work?
Read out and check GPIO and SPI registers (compare to working "instances")
JW
2020-03-01 7:06 AM
Yes, SCK work.
Also, I detected with the scope another strange bahaviour;
as you know, each SPIx_SCK pin has some alternative GPIO options;
for SPI4 I detected that SCK is provided on two GPIO at same time (when it is configured only on PE2 ¿? )
the SPI4 is configured to provide its SCK output on PE2, but the SCK signal is visible with the scope on PE2 and PE12; but PE12 is not configured at all!
I tested my own program code (you can see initialization code upside, the software chip select for SPI4 is set to PC10, not PE2; sorry for the mistake)
and the firmware examples for NUCLEO-H743ZI; on both the only working SPI is SPI1, if I change the example code to use SPI3 or 4, it performs the same way.
SPI 2 is not tested, but the interest are for SPI 3 and 4. These need to be used on a ready routed and manufactured PCB.
Thanks for the answers,
2020-03-02 1:10 AM
the board is a NUCLEO H743ZI2
2020-03-02 1:49 AM
Read out and check GPIO and SPI registers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.