2014-06-26 6:07 AM
Hi,
I am using STM32l151vbt6 MCU and I am trying to configure RTC Alarm for ever 15th minute that is 0, 15, 30 and 45th minute of the every hour. I can configure the Alarm and it will work for the first time, If I try to set it again after the alarm occurs, it would set to previous alarm state. If i reset the MCU i can set the alarm and it will wake the controller from the stop mode when the alarm occurs, Please let me know how can i set the next alarm without resetting the MCU.Alarm Configure Code:/*~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~*/ /* 8(hour) and 19(day) are masked and there is no effect on the alarm */ RTC_AlarmTypeDef RTC_AlarmStructure = { 0, 0, 0, RTC_H12_AM, (RTC_AlarmMask_DateWeekDay | RTC_AlarmMask_Hours), RTC_AlarmDateWeekDaySel_Date, 19 }; const uint32_t alarm_interval[4] = { 15, 30, 45, 0 }; /*~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~*/ RTC_Read(); RTC_AlarmStructure.RTC_AlarmTime.RTC_Minutes = alarm_interval[RTC_current_time.minute / 15]; RTC_Alarm_Config(&RTC_AlarmStructure);void RTC_Alarm_Config(RTC_AlarmTypeDef *RTC_AlarmStructure){ /*~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~*/ EXTI_InitTypeDef EXTI_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /*~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~*/ RTC_AlarmCmd(RTC_Alarm_A, DISABLE); /* EXTI configuration */ EXTI_ClearITPendingBit(EXTI_Line17); EXTI_InitStructure.EXTI_Line = EXTI_Line17; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); /* Enable the RTC Alarm Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = RTC_Alarm_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); RTC_SetAlarm(RTC_Format_BIN, RTC_Alarm_A, RTC_AlarmStructure); /* Clear RTC AlarmA Flags */ RTC_ClearITPendingBit(RTC_IT_ALRA); /* Enable AlarmA interrupt */ RTC_ITConfig(RTC_IT_ALRA, ENABLE); /* Enable the alarmA */ RTC_AlarmCmd(RTC_Alarm_A, ENABLE);}Alarm ISR: EXTI_ClearITPendingBit(EXTI_Line17); if(RTC_GetITStatus(RTC_IT_ALRA) != RESET) { /* Clear RTC AlarmA Flags */ RTC_ClearITPendingBit(RTC_IT_ALRA); } #rtc-alarm2014-06-26 8:16 AM
On other STM32 parts I've just advanced the settings in the register.
Perhaps you've not cleared the interrupt/exti properly, but I can't tell from your code.2014-11-24 5:12 AM
Hi Clive,
Thanks for the reply. You can have a look at my code.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.