2010-02-05 1:52 AM
STM32 RMII ethernet clock
2011-05-17 4:39 AM
General update.
We have a valid ethernet link established and the library reset functions that interface with the MAC require a functioning and correctly clocked PHY so reset.
Currently in the process of porting the STM32 uip demo to Crossworks 2, on the STM32 so will update this thread when I get a full TCP/IP stack running.
2011-05-17 4:39 AM
>Currently in the process of porting the STM32 uip demo to Crossworks 2, on >the STM32 so will update this thread when I get a full TCP/IP stack running.
Any news about success with your Webserver ? Currently I also have to choose a Phy. While the Hitex Comstick uses a (very MII compatible) STE100, the stm3210C-Eval and many others use Nationals DP83848 with RMII. As far as I can understand, RMII requires additional 50Mhz Oscillator at X1 why the RMII can be hardly recommended if the F107 IO pins for MII are not occupied ?
2011-05-17 4:39 AM
Hi,
We got our system working. Issues that we faced were Stack overflow (worth implementing real time stack monitoring) and also ensuring that while a packet was in the transmit buffer we held off/checked to see that the buffer was available before loading a second packet.
With the RMII clock we ended up running the STM32 at 36MHz and using an external 50MHz clock on the phy - which worked for us.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.