2020-10-29 11:51 PM
Hi All,
We are planning to use STM's STM32H750VB in our design.
We need 1 QSPI port from the MCU.
We saw in the reference manual following 2 things:
1. In block diagrams (page 883) it is mentioned as if we can enable dual-flash mode (8 bits) and disable dual-flash mode (4 bits).
2. In QUADSPI main features section (section no. 23.2), it is mentioned like '8, 16, and 32-bit data accesses are allowed'
So whether we can use only 4 bits (either Bank1 or Bank2) or we should use all 8 bits (both Bank1 & Bank2) ?
What about chip select connection ?
Best Regards,
Madhusoodana Bairy
2020-10-30 12:41 AM
1 & 2 are about different things
Generally you'd pair them (dual) to improve the bandwidth. Works with a single chip select.
Check the H7 DISCO boards, definitely examples. See H750B-DK schematic
2020-10-30 1:18 AM
Thanks for your response clive1.
What about following statement in reference manual(section no. 23.2): "8, 16, and 32-bit data accesses are allowed"
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.