2022-04-04 9:55 PM
Hi all,
I am using a custom board designed using mcu STM32 L071CZ. I want my device to go to stopmode afte doing a certain task. I checked the current consumption in run mode, it is almost 4.7mA and in stop mode in 3.56 mA.I haven't enabled any other peripheral in mcu except rtc.(RTC only enabled) . Ihave checked the PCB design, there are no way for current leakages. In data sheet, consumed current is said less than 100 uA.
Code I used for checking.
*******************//code 1 *******************************************************
count=count+1;
HAL_Delay(10000);
//Entering stopmode
HAL_SuspendTick();
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
HAL_ResumeTick();
SystemClock_Config();
2022-04-11 6:20 AM
Hello @Praththanan ,
I checked your code on NUCLEO-L073R. I got the good values, RUN~4mA and STOP~100µA.
How do you want to wakeup the chip ?
On your PCB what is powered ON?
Best regards
2022-04-11 6:31 AM
LEDs, other peripherals?
What about STANDBY?
Entering WFI loop again after servicing other interrupts?
With/without debugger attached?
Able to output any info/diagnostics via a serial connection to better understand internal states/actions?
2022-04-14 8:23 PM
Hi @Simon.T , thank you for responding. I tried to power up PCB using battery and tried to power up mcu using 3.3v pin.
in stm32l0xx.it.c.....
void RTC_IRQHandler(void)
{
/* USER CODE BEGIN RTC_IRQn 0 */
/* USER CODE END RTC_IRQn 0 */
HAL_RTCEx_WakeUpTimerIRQHandler(&hrtc);
/* USER CODE BEGIN RTC_IRQn 1 */
wakeup = wakeup + 1; ## Here initiating a variable and using it in main.c file
/* USER CODE END RTC_IRQn 1 */
}
I am wake up mcu using this.
Is there any other way to wakeup.
I tried this way also.
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0xB4AA, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
/
2022-04-14 8:27 PM
Hi @Community member , thank you for replying,
There are no LED working as I didn't enable any peripheral (enabled only RTC).
I have removed the debuggers.
I haven't tried any way to output any info. Can you tell me how can I read without using live expression?
2022-05-01 5:02 PM
Before going to the low-power mode, set the DBG_CR register to zero and disconnect the debugger physically.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.