2020-06-04 12:32 PM
Hi everyone.
So my previous post just did not load for some reason.
The problem is that for some reason I get this issue when I debug once I enable the interrupts.
I am simply trying to respond on the TIM5 interrupt but I get thrown to a part of the file startup_stmf32f401retx.s to this line of code:
/**
* @brief This is the code that gets called when the processor receives an
* unexpected interrupt. This simply enters an infinite loop, preserving
* the system state for examination by a debugger.
*
* @param None
* @retval : None
*/
.section .text.Default_Handler,"ax",%progbits
Default_Handler:
Infinite_Loop:
b Infinite_Loop Now it seems like it's suppose to help me analyse whats going on inside an interrupt but I didn't have any breakpoints set in the project yet? This is the Stack Trace.Thread #1 [main] 1 [core: 0] (Suspended : Signal : SIGTRAP:Trace/breakpoint trap) UsageFault_Handler() at startup_stm32f401retx.s:101 0x8000630 () at 0xfffffff1 0x0 () at 0xfffffff9 stepper_init() at stepperpwm.c:18 0x80001ea main() at main.c:38 0x8000530 Reset_Handler() at startup_stm32f401retx.s:83 0x8000616
Finally here is my code... I like to try it baremetal before I start using MCU specific headers for the most part. main () { housekeeping_init(); while(){ housekeeping(); } } void housekeeping_init(){ __disable_irq(); RCC->AHB1ENR |= 1;//(1 << 0); //TIM5 RCC->APB1ENR |= (1 << 3); TIM5->PSC = 1000-1; TIM5->ARR = 10-1; TIM5->DIER |= 1; NVIC_SetPriority(TIM5_IRQn,2); NVIC_EnableIRQ(TIM5_IRQn); GPIOA->MODER |= 1; __enable_irq(); TIM5->CR1 |= 1; } void TIM5_IRQHandler(){ //TIM5->SR &= ~(1); TIM5->SR &= ~0x01; //TIM5->SR = 0; GPIOA->ODR ^= 1; ***++; } void housekeeping(){ if (*** == 300) { GPIOA->ODR ^= 1; } }
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.