2008-11-19 2:24 AM
STM32 in Arduino Format
2011-05-17 3:52 AM
Hello
We have cooked up an STM32 board in Arduino format. After hours of wrestling with possible names, we ended up mashing Cortex and Arduino to make Cortino. At least we didn't call it the Artex ;) Details here: As you would expect, the Cortino can be flashed via the USB port. One neat feature is access to the serial JTAG debugger from the USB port, so you should be able to debug the thing with no additional hardware once we have gotten the SWJ-DP stub finished. Just in case, we also have a full 20-way JTAG port on board... Getting an open source GDB stub and/or OpenOCD stub would be a real win for the community. So I would love to here from any expert out there on SWJ-DP who would like to have his name carved in open-source immortality. Tim2011-05-17 3:52 AM
Quote:
At least we didn't call it the Artex ;)
Or the Cortina :-W :DWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.