2018-01-17 12:33 PM
Hello,
I've have the I2C example code I2C_TwoBoards_ComIT working between an F722 board and a F303 board. That example passes a fixed size character buffer between the two boards fine. As I start to modify the code for my usage of variable sized buffers, it fails because the buffer size is not known.
What I want is an I2C receive interrupt after a random size (less than max size) buffer is received. Or even a partial packet packet received. I will copy the I2C rx buffer to my own ring buffer to handle verification and construct the logical packets I'm dealing with.
Is there a configuration flag(s) that allows this type of interrupt driven behavior? Or should I be using a different approach?
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.