2011-08-28 1:37 PM
Hello guys,
I spent all the afternoon trying to just trigger an interrupt. The example is easy, I have FreeRTOS 7.0.1 running with a periodic task which writes a sequence towards USART2 employing the DMA1 (channel7). The transfer is successful as I can read it in the PC Serial Port, but the interrupt informing the transfer completed never occurs. The code is the next: main.c: #define DMA_Channel_USART2_RX DMA1_Channel6 #define DMA_Channel_USART2_TX DMA1_Channel7 #define DMA_FLAG_USART2_TC_RX DMA1_FLAG_TC6 #define DMA_FLAG_USART2_TC_TX DMA1_FLAG_TC7 void send_USART_dma(const uint8_t *buff, uint8_t size) { DMA_InitTypeDef DMA_InitStructure; /* shared DMA configuration values */ DMA_InitStructure.DMA_PeripheralBaseAddr = &(USART2->DR); DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;DMA_InitStructure.DMA_MemoryBaseAddr = buff;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_DeInit(DMA_Channel_USART2_TX); DMA_Init(DMA_Channel_USART2_TX, &DMA_InitStructure); DMA_ITConfig(DMA1_Channel7, DMA1_IT_TC7, ENABLE); DMA_Cmd(DMA_Channel_USART2_TX, ENABLE); USART_DMACmd(USART2, USART_DMAReq_Tx, ENABLE); //while (DMA_GetFlagStatus(DMA_FLAG_USART2_TC_TX) == RESET) { ; } <- Here I want the interrupt instead an active waiting } void initUSARTs(void) { GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); /* Configure USART Tx as alternate function push-pull */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure USART Rx as input floating */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2, ENABLE); } void blinkingLed(void *pvParameters) { portTickType xLastWakeTime = xTaskGetTickCount(); unsigned led_on = 0; for(; { led_on = ~led_on; if(led_on) GPIOC->BSRR |= 0x00001000; else GPIOC->BRR |= 0x00001000; vTaskDelayUntil(&xLastWakeTime, (500 / portTICK_RATE_MS)); } } void countdown(void *pvParameters) { portTickType xLastWakeTime = xTaskGetTickCount(); uint8_t count[] = {0x44, 0xFF, 0x55}; uint32_t entero32 = 0x11223344; for(; { send_USART_dma(&entero32, 4); vTaskDelayUntil(&xLastWakeTime, (1000 / portTICK_RATE_MS)); } } void iDMA1_Channel7_IRQHandler(void) { DMA_ClearITPendingBit( DMA1_IT_TC7); DMA_Cmd(DMA_Channel_USART2_TX, DISABLE); USART_SendData(USART2, 0x99); } int main(int argc, char *argv[]) { initLEDs(); initUSARTs(); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); NVIC_InitTypeDef NVIC_InitStructure; NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2); NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel7_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); //NVIC_EnableIRQ(DMA1_Channel7_IRQn); <- I guess this is done in NVIC_Init // Creating tasks xTaskCreate(blinkingLed, ''Task 1'', 240, NULL, 1, NULL); xTaskCreate(countdown, ''Task 2'', 240, NULL, 1, NULL); vTaskStartScheduler(); return 0; } Some info to avoid pasting more trivial code, the Handler is well attach to the interruptVector and I could run a Timer interrupt with the same steps as in this code. Do you what is happening? Thanks in advance.2011-08-28 2:14 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.