2015-02-08 8:25 AM
Hi,
I'm STM32F4-Discovery board and am trying to log GPS data into uSD card. I've configured the DMA and am able to view the data in the card. But, the data has gaps which was expected as the DMA interrupt is count based. To avoid this I'm using Timer 2 to detect any transitions on the Rx line and configured the timer to reset mode. I want the transition on the line to reset the timer and start the count. Only on no activity, the timer would overflow and generate an interrupt. Basically, some kind of time out interrupt. However, the timer overflows and continuously generates the Update interrupt even when there is not activity on the line. Here is the code I've used... Can you help where I went wrong.. Thanx in advance void GPS_Gap_Timer_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; TIM_TimeBaseInitTypeDef TIMER_InitStructure; TIM_ICInitTypeDef TIM_ICInitStruct; NVIC_InitTypeDef NVIC_InitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA , ENABLE); // PA8 = TIMER2_CHANNEL-1 GPIO_PinAFConfig(GPIOA, GPIO_PinSource15, GPIO_AF_TIM2); // Configure Port-A GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); TIM_InternalClockConfig(TIM2); // Choose Internal Clock for Timer2 TIMER_InitStructure.TIM_CounterMode = TIM_CounterMode_Up; // Choose Up Mode Count TIMER_InitStructure.TIM_ClockDivision = TIM_CKD_DIV4 ; // 36MHz / 4 = 9MHz TIMER_InitStructure.TIM_Period = 55000; TIMER_InitStructure.TIM_Prescaler = 0; // 36MHz TIM_TimeBaseInit(TIM2, &TIMER_InitStructure); TIM_ICInitStruct.TIM_Channel = TIM_Channel_1; TIM_ICInitStruct.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStruct.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStruct.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStruct.TIM_ICFilter = 0; TIM_ICInit(TIM2, &TIM_ICInitStruct); TIM_UpdateRequestConfig(TIM2, TIM_UpdateSource_Regular); TIM_SelectInputTrigger(TIM2, TIM_TS_TI1F_ED); TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Reset); TIM_ClearITPendingBit(TIM2,TIM_IT_Update); TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); TIM_ITConfig(TIM2, TIM_IT_Trigger, DISABLE); NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1); TIM_Cmd(TIM2, ENABLE); }2015-02-08 8:43 AM
So what speed is the bus clock, and what speed is the time base? What is the time out?
This does sets a filter speed, it's not a prescaler for the timerTIMER_InitStructure.TIM_ClockDivision = TIM_CKD_DIV4 ;
Wouldn't the reset perhaps cause an update interrupt? You could use the CCx instead of the Update, still it's likely to hit if you have a short period and the counter wraps. Could you not use the 32-bit range of the counter?2015-02-08 8:38 PM
Thanks a lot for the reply...
True... I realised later that it is supposed to generate the update interrupt because the timer is configured in reset mode... So it'll reset on trigger.. otherwise its running and would generate an update on overflow... The time is suffecient because data is 115200bps and I've given about 10 bytes gap... I think I'll have to enable update interrupt only after triggering once... I'll try with 32-bit and revert back on the status...2015-02-08 10:42 PM
I'm not sure what you mean by gaps. Missing data?
GPS devices tend to output data in bursts at the top-of-second, this might be half a dozen NMEA sentences, but likely less than 11520 characters which a full second of solid data might provide.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.