2018-03-23 9:15 AM
I understand a high speed CAN bus bit error means that while I am transmitting a bit outside of the arbitration period I sense the opposite bit on the bus. However STM gives two bit errors: 'bit dominant error' and 'bit recessive error', and I'm not sure what they each mean:
Does 'bit dominant error' mean 'While I was transmitting a dominant bit the bus was sensed as recessive' or does it mean 'While I was transmitting a recessive bit the bus was sensed as dominant' ?
Thanks
2018-03-23 9:30 AM
I may have found the answer by experiment:
Shorting the CAN-H and CAN-L causes a bit dominant error - implying the meaning is
bit dominant error = 'while transmitting a dominant bit the receiver sensed a recessive bit'.
bit recessive error = 'while transmitting a recessive bit the receiver sensed a dominant bit'
2018-03-23 11:06 AM
Actually I think means some else's dominant bit dominates yours.
2018-03-23 1:36 PM
I think the opposite - but just based on experimental observation. A shorted CAN bus would have 0 differential voltage which would appear as a recessive bit to someone observing the bus, and I find if I short the CAN bus I see '
bit dominant error', which implies that the error is telling me that when I tried to transmit a dominant bit I read a recessive bit.
In fact I have not seen any 'bit recessive errors' in any of our 50k + deployed devices - which makes sense because if electrically the bus is screwed up to override your recessive bit transmissions I think you'd never make it past bus arbitration to where you could register a bit error.
In any case, in case anyone is interested 'bit dominant error' is, among other things, a sign that you might have (intermittent) short circuits between the CAN-H and CAN-L.
On the other hand if CAN-H or CAN-L go open circuit I see 'stuff' and 'form' errors.
2018-03-23 6:16 PM
The STM32 applies a state via CAN_TX, and observes the bus state on CAN_RX.
Multiple devices can drive the bus and the protocol is designed so you can see if you lost to a device with a more important message ID. The loser backs off.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.