2011-04-13 2:29 AM
STM32 and external (S)DRAM
2011-05-17 5:31 AM
Can't be DRAM, must be SRAM. You can get 8M (4M x 16) e.g. CY62187EV30.
This seems an ambitious project for a microcontroller such as the STM32 which isn't really that suited to running code from external memory.2011-05-17 5:31 AM
Thank you for the info about the SRAM module.
Why is the STM32 not suited to running code from external memory?
Do you see other options to run code from a SD-Card (or maybe an other Cortex-M3 microcontroller which is better suited for such thing)?
Greets
Christoph
2011-05-17 5:31 AM
Because external bus access is relatively slow, and the part doesn't have a cache.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.