cancel
Showing results for 
Search instead for 
Did you mean: 

STM23f303-re vs STM32F303-ze virtual comm port

DPeki.1
Associate II

Hello,

I have a project working on the F303-re Nucleo board. I want to run it now on the F303-ze Nucleo board. Apparently virtual com port doesn't work the same on the ZE as it does on the RE. I can take a new RE board, copy the binary file to the RE board and the app starts communicating on the virtual comm port. I do the same thing on the ZE board and I get no virtual comm port communications.

I assume I'm missing a jumper or solder bridge configuration that will allow the ZE to start virtual comm port communications. What am I missing?

Thanks,

  • Dave

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @DPeki.1​,

A similar question is already asked here. And the best answer is already provided by @Peter BENSCH​. 

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Imen.D
ST Employee

Hello @DPeki.1​ and welcome to the Community :),

Do you see the device in your device manager as serial interface?

Maybe that issue is linked to the ST-Link firmware version.

So, try to upgrade the ST-Link firmware version, then disconnect and connect your board.

Have a look at the AN4879 USB hardware and PCB guidelines using STM32 MCUs, it may help you.

When your question is answered, please close this topic by choosing Select as Best.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
DPeki.1
Associate II

Yes Imen,

It does show up as a serial interface (Comm 5). And the file exloper shows the device as Nod-f303ze. That looks the same as a F722ze board that I have where the virtual comm port works correctly (comm 7 and a different device name in file explorer - f722 vs f303). On the 722, solder bridges SB132 and sb133 have been removed. Those relate to USB useage, not virtual comm port as I read it, right?

Should I be able to load exactly the same bin file between the 303re and the 303ze? I would assume so since they're the same processor.

I will look at the document you referenced.

Thanks,

Dave

DPeki.1
Associate II

I guess the basic question is should code that runs on the f303re run on the f303ze? Can I load the same binary on both boards and expect the same operation? If the answer is yes, I've got a bad ZE board. If the answer is no, I need to track down the differences. (I know the connector layout is different.)

KDJEM.1
ST Employee

Hello @DPeki.1​,

A similar question is already asked here. And the best answer is already provided by @Peter BENSCH​. 

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.