2013-12-11 4:57 AM
Is it possible to install/use the STM Virtual COM Port on Windows 8?
#windows-82013-12-11 8:29 AM
Probably, if the driver is unsigned you'll need to turn off that test for it to load/work.
2013-12-13 1:55 AM
I tried turning off the signed driver protection. It didn't help. I have also tried running the driver in compatibility mode and as administrator. No luck.
2014-01-26 10:51 PM
Good news: I upgraded the Windows 8 computer to Windows 8.1 and the STM Virtual COM Port now successfully installs and works. It is not ideal that I cannot use Windows 8 without the upgrade, but it is still great that the driver does work on a version of the newer OS.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.