2010-09-23 4:00 PM
STM USB Library Bug? Gets stuck in interrupt
2011-05-17 5:08 AM
I'd guess you could check for and clear/disable the interrupt as it is about to leave the ISR.
Or ascertain why it is getting set or why it is not being cleared by the ISR. If the ISR does not address the condition (due to code flow issues, or whatever), you'll just get an interrupt crap storm and nothing else will run.2011-05-17 5:08 AM
I still cant put my finger on the cause of this. It has something to do with writing to a IN endpoint when the PC doesn't read from it. It definitely gets stuck in an ''interrupt crap storm''. I really don't have time to try find the cause of it now but I think I am going to have to as it is starting to plague me a little!
I'll be honest, I am a little over fumbling my way through this USB stack. There is no documentation and limited examples and now problems that cause it to get stuck!!! But, I suppose it would have taken me forever to even get this far on my own!!!
2011-05-17 5:08 AM
Hi
Are you using the Virtual COM driver? If so, I had a similar issue, but created a work around. The problem is that the 'output' buffer gets 'full' and effectively locks up the chip due to the ISR being fired continuously. The workaround (in my case specifically using usb stdio via vcom) involves polling for information to see if there is anything in the transmit buffer. If the polling fails after x attempts (1000 in my case), the call to transmit is silently ignored. I will post some code later explaining this better :)2014-01-06 4:41 AM
Hi leppie,
I am having the same problem!Could you share your solution?Thanks :)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.