2017-07-18 4:27 AM
stm microcontroller reset cicuit i want
2017-07-18 6:27 AM
Try to formulate questions with clarity and context.
Review some of the schematics for EVAL and DISCO boards.
The internal POR circuit expects to see a supply across VDDA and VSSA.
If you have a system with multiple supply rails, consider how they rise, and consider thresholding parts like the MCP-120.
2017-07-19 11:20 PM
Thank you
2017-07-19 11:27 PM
8051 I/O pin current rating is 10mA.
AVR I/O pin current rating is 20mA.
what is the I/O pins current rating for STM32. and also how implement the BROWN OUT Reset?
2017-07-20 7:13 AM
Study the Data Sheet and Reference Manual for your device.
2017-07-20 7:19 AM
yeah. I saw datasheet its 25mA for I/O pins.
when program counter Overflow occur?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.