2023-07-21 7:26 AM
I would like to know the connector CN1 the daughter board for stlink v3
I am attaching an image for reference. Kinldy anyone share the part number
2023-07-22 12:39 AM
2023-07-22 9:11 AM
Could also check BOM from NUCLEO-144 boards using ST-LINK/V3, so H743ZI2, H723ZG
Header 5x2, 1.27mm, Dual row, Straight, Surface mount, vertical male connector. 3.05mm lead. Mates with FFSD connector. Footprint compatible with FTSH-107-01-L-DV,-K,-A,-P,-ES (STDC14 MEDIUM)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.