2015-11-05 1:21 AM
hello
as required in the STemwin manual i have to enable RCC AHB1 CRC clock. ''The CRC module (in RCC peripheral clock enable register) should be enabled before using the library''trying to use RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_CRC, ENABLE);as it apears at AN4323,i get error ''identifier undefined'' and ''function declared implicitly''how i enable that?2015-11-05 2:03 AM
Hi Assaf,
1- What are you using as STM32 product?2- You are using SPL or HAL libraries?You need to check the correct function to enable CRC clock.-Syrine-2015-11-05 4:06 AM
Thank you for your reply.
1. I'm using STM324x9I-Eval with Himax Driver LCD.2. I'm using HAL Libraries and found that Define. __HAL_RCC_CRC_CLK_ENABLE();is that correct? if yes -
i still have problems using MEMDEV.2015-11-05 4:41 AM
Hi Assaf,
Yes it is the correct function. But now please explain with more details the new problem.I'd highly recommend you to have a look to STemWin examples under STM32Cube F4 package: STM32Cube_FW_F4_V1.9.0\Projects\STM324x9I_EVAL\Applications\STemWin, it can be very useful.-Syrine-2015-11-05 5:40 AM
I'm drawing bitmap to the screen, its taking time and i have flickering - video attached.
i'm trying to solve that by using MEMDEV, but i can't see any change. here is the flow: 1. create 1 memory device. 2. select the relevant handle. 3. drawing anything to it. 4. copy to lcd. what happens is, writing to MEMDEV writes to the screen as well, before copy to LCD. GUI_MEMDEV_Handle hMemDev1= GUI_MEMDEV_Create(0,0,240,320); GUI_MEMDEV_Select(hMemDev1); GUI_SetFont(&GUI_FontOpenSansRegular27); GUI_SetColor(0x42CADE); //GUI_SetBkColor(0x2A2A2A); GUI_DispStringHCenterAt(''WRITE'' ,(LCD_GetXSize()/2),28); GUI_MEMDEV_CopyToLCD(hMemDev1);. iv'e also tried to GUI_Draw_Bitmap() and its acting the same. Thank you for your help. ________________ Attachments : TRIM_20151104_091451.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtWJ&d=%2Fa%2F0X0000000aRC%2FZQcglF_htDv_9L8YB03S8J.CVMvIkFc_ZdydqU2EbbQ&asPdf=false2015-11-06 12:48 AM
Hi Assaf,
I would like to give you some advices that can be useful: 1- The use of ''multi-buffering'' functionality to avoid flickering effect: · Add the enable of multi-buffring functionality to your application: WM_MULTIBUF_Enable(1); · update ''LCDConf.c'' file => #define NUM_BUFFERS 32- To accelerate the bitmap drawing, it is recommended to use the Chrom-ART Accelerator.-Syrine –2015-11-07 10:45 AM
I do use multi-buffering as you adviced, and that's how its looks, in the video. thats why im trying the MEMDEV option.
can you refer me to some example of how to use Chrome-ART?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.