2015-10-29 9:46 AM
Hello
Currently i work with the HAL lib where i can graphically setup the system clock of my STM32F4xx controller. I do have to set up the same libraries i wrote (mostly copy paste except interface commands,.. ) in a project file using the StdPeriphLib exept the hal libI'd like to set up the system core frequency through PLL at 100MHz like i did it with the graphic Cube configurator. Which file and which commands do i have to edit to achieve my goal? Also, id like to set up all the clock prescalers exactly the same like in HAL.Next problem is, when i run the project in the debug mode with the default settings (no idea which clock speed) i can set breakpoints in e.g. the startup file but not in my main file or other files. what could cause that?2015-10-29 11:15 AM
The PLL and clock setting for the SPL live in the system_stm32f4xx.c file, SetSysClock(). There might be an Excel sheet to do it, but it's math a 10 year old could do, it's not that complicated, the interrelationships are diagrammed in the Reference Manual.
No idea what tool chain you're using. Some tools stop you placing break-points where the code doesn't exist on the target. ie routine is never called, linker does dead-code removal.2015-10-29 11:24 AM
hi clive
thanks for your quick answer.im gonna check the file tomorrow. and for the debug problem: im using keil v5 with a nucleo board where the st link programmer is onboard.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.