2018-04-12 9:01 PM
I am using the IAR compiler with the Cortex-M3 EVB board. I am trying to upload a simple USART Firmware on the EVB board using the Standard Peripheral Library. If you add a file to the startup code file (even though I did not add it), the system timing will be faster and the USART will not work properly. (MAKE works well without warning or error.) What's wrong?
I am using the STM32F103RBT6 chip.
Internal clock 8MHZ is used and no PLL is used.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.