2022-04-01 11:29 PM
i recently purchase STLINK V3 MODS i connect using SWD connection as STLINK V2 .
i am using stm32cubeprogrammer for programming when i press connect it gives error
st link error DEV_TARGET_CMD_ERROR .
what is the problem and how can i solve it?
2022-08-12 5:31 PM
I have same situation. I tried to look up any solutions , but nothing.
2022-08-12 5:42 PM
Very little meat here to work from.
What STM32 model are you connecting too?
Custom board? Good wiring and grounds?
The ST-LINK/V3 need a high quality USB cable, cheap/charger cable are often no good. Have some marked/rated for USB 2.0 480Mbps operation,will likely be wider and have shielding.
Speed of SWD can also now exceed that of some STM32 parts, ie CM0(+) ones
Make sure your interface connects NRST for the "Connect Under Reset", etc to actually do anything.
Find some diagnostic skills, it will help
2022-08-12 6:42 PM
It seems to me, that if you solder the pin "T_Vcc" (pin 30) the error message will be disappeared , but the programer would not works. :(
2022-08-16 12:42 PM
I try to use STM32F103C6., blue pill modul.
I worked with this modul earlier. I programmed with a clone stlink-V2 via 3 pin. It was everything ok, but I updated STMCube, unfortunately. :(
After the update I couldn't download the new firmware to the clone programmer. I bought a St V3 programmer , and there is not a correct description which pins need to use, which pins are optional. Let's it hang...
So, thank you for your advitice! I will try to use nrst pin.
I thing the usb cabel is good, because StmCubeMx is recognize the IC type. But I will change it too.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.