2025-02-12 1:46 AM - last edited on 2025-02-12 1:56 AM by Andrew Neil
Dear all,
i am facing very strange problem with sprintf function .
i am using sprintf function in 1ms timer interrupt routine and it works fine. for example.
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
sprintf(uDisMsg, "%.1f", 258.6);
sprintf(lDisMsg, "%.1f", 25.3);
printf("%s %s\n",uDisMsg,lDisMsg);
}
but when i call any method from while(1) loop in main function like
while (1)
{
superloop();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
then sprintf sometimes outputs right result sometimes outputs to 0.0
if i don't call superloop() in while(1) then sprintf works fine.
i am not able to understand what problem it faces while calling any method in while(1).
Code formatting applied - please see How to insert source code for future reference.
2025-02-12 1:55 AM
@sanju wrote:i am using sprintf function in 1ms timer interrupt routine .
That's not wise at all - especially on a chip with no FPU.
Plus you are also calling printf - is that a blocking call to output the data over a UART?
These are really not things to be doing in an interrupt handler!
@sanju wrote:i am not able to understand what problem it faces while calling any method in while(1).
Probably, you just get away with it in the case with no code in the main loop ...
2025-02-12 2:11 AM
printf can be removed, that is not part of application it is just used to see output of sprintf.
this code works on STM32F072RBT7 but doesn't work on STM32F103RBT7.
and sprintf doesn't have any problem with %d format specifier, it only creates problem with %f.
2025-02-12 2:17 AM
@sanju wrote:and sprintf doesn't have any problem with %d format specifier, it only creates problem with %f.
As previously noted, you're on a processor with no FPU - so all floating-point stuff has to be done "manually" in software.
@sanju wrote:this code works on STM32F072RBT7 but doesn't work on STM32F103RBT7.
Again, it's probably marginal - you just happen to "get lucky" in one case, and not the other.
Just don't do this in an interrupt handler!
@sanju wrote:printf can be removed, that is not part of application it is just used to see output of sprintf.
But none of it makes sense to be in a real application!
What is it you're actually trying to achieve here?
2025-02-12 2:37 AM - edited 2025-02-12 2:37 AM
@Andrew Neil wrote:
As previously noted, you're on a processor with no FPU - so all floating-point stuff has to be done "manually" in software.will do it.
@Andrew Neil wrote:Again, it's probably marginal - you just happen to "get lucky" in one case, and not the other.
Just don't do this in an interrupt handler!
Ok.
@Andrew Neil wrote:But none of it makes sense to be in a real application!
What is it you're actually trying to achieve here?
I need to convert variables into string so that it can be displayed on 7segment display.
i can remove the stuff like sprintf from interrupt handler.
i am trying understand why it is creating problem while calling any method from in while(1).
Thanks for the guidance, i will do this out of interrupt handler.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.