2017-09-13 5:09 AM
I just found this out on electronics stackexchange:
If you set the struct member NVIC_IRQChannelCmd = DISABLE, calling NVIC_Init() will do nothing to set the interrupt priority and sub-priority. If you want the interrupt disabled initially and you want to use NVIC_Init(), you will have to enable the interrupt with the struct and then disable it explicitly after calling NVIC_Init() by calling NVIC_DisableIRQ().
Why does NVIC_Init() skip configuring the interrupt priority and sub-priority if the interrupt is to be disabled initially? After seeing the problem on the other forum, I reviewed my own code and found a couple places with the same 'mistake'.
I think it would be dangerous for me to fix NVIC_Init() and recompile the SPL, since the problem would be back with the next download. I think an alternate solution would be to skip using NVIC_Init() and instead use the CMSIS functions: NVIC_EncodePriority() and NVIC_SetPriority() followed by either
NVIC_DisableIRQ() or
NVIC_EnableIRQ().
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.