2012-02-01 6:17 AM
2012-02-01 6:48 AM
So why wouldn't sending a zero byte achieve exactly what you want?
Half-duplex means the input/output are connected together. Sending ''nothing'' is a bit vague, people here would look at the datasheet if they could guess what part you're talking about.2012-02-01 8:16 AM
Now according to the datasheet I don't want send anything ( don't send this dummy byte) , I want only play with the clock and receive the values because my MOSI line should stay at ''0''.
What do I have to do ?
you have to read the SPI standard Erik
2012-02-05 3:51 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.