2008-08-17 10:46 PM
solved : function __RESETPRIMASK(); firmware library
2011-05-17 3:29 AM
Hello,
I'm using the firmware library, Where can i find the functions __RESETPRIMASK(); __RESETFAULTMASK(); __SETFAULTMASK(); __GetBASEPRI() thanks [ This message was edited by: julien.massot on 09-04-2008 12:14 ]2011-05-17 3:29 AM
cortexm3_macro.s
2011-05-17 3:29 AM
Thanks
2011-05-17 3:29 AM
hi!
i am a very very hobby like starter, the cortex is actually the first microcontroller i am playing with... i got the LED example working and now want to read a PWM signal from a MaxSonar range sensor, so I started looking at the PWM input example, but I struggle compiling it. first I found out that I was missing the cortexm3_macro.s file, so I put it in the directory. but now, i dont know how to make/build it. when i just compile the .s file, i get loads of errors saying that the symbol is already defined?! here some example output: cortexm3_macro.s:69: Error: symbol `Input' is already defined cortexm3_macro.s:69: Error: bad instruction `none' cortexm3_macro.s:70: Error: symbol `Return' is already defined cortexm3_macro.s:70: Error: bad instruction `none' cortexm3_macro.s:71: Error: junk at end of line, first unrecognized character is `*' cortexm3_macro.s:72: Error: bad instruction `__sev' cortexm3_macro.s:77: Error: junk at end of line, first unrecognized character is `*' maybe someone want to have a look in my makefile... thx a lot chaps, dan2011-05-17 3:29 AM
Haven't checked your makefile but it's probably correct. The problem is that you seem to be using the wrong cortexm3_macro.s. They are tool specific and since you use GCC you should take the one from project/Ride. Or use my attached cortexm3_macro.h instead of the one from the library and avoid using an assembly file at all. Plus you might save a few bytes flash :-]. I won't guarantee that it's bug-free, but well, the library isn't either. Please post any corrections.
2011-05-17 3:29 AM
great, thx for the help and hints! am at work at the moment, but will try later and post results, im sure im not the only one struggeling with that ;)
Cheers, DanWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.