2014-05-21 5:09 AM
Is below is right way to send STM32F205RBT6 in sleep mode:
I have to do some task, then send MCU in sleep mode for 1 sec & then again execute those tasks.main(){ while(1) { // do some task configure_timer_1_sec(); //configure interrupt when 1 sec completes __wfi(); }}timer_isr(){ clear_interrupt_flag();}2014-05-21 9:27 AM
Hi
I am not familiar with the part you are using. __wfi() is definitely the ARM command to put the processor into sleep mode (as defined by ARM). The short code you showed does not show all the setup that should be done to get the most power saving. For instance, on the STM32F405 part that I have implemented power save on, the peripherals can be clock gates (select which peripherals still get clocked during sleep mode) - this really saves power.2014-05-22 1:36 AM
First I am trying to send CPU in sleep mode. I am not worried about peripherals now.
So I initialized a timer to 1 sec interrupt & then used __wfi().So when MCU has 1 sec timer interrupt it wake up & start executing next instructionEDIT: is there any specific register in which we can select which peripherals can be clock gated or its jusy by enabling clock to peripherals2014-05-22 1:56 AM
''So I initialized a timer to 1 sec interrupt & then used __wfi().
So when MCU has 1 sec timer interrupt it wake up & start executing next instruction'' Generally, yes. However testing it is a problem. When you use a debugger - the processor is not actually suspended (clock stopped). Probably, the easiest way is to have your main loop toggle an LED. When the processor goes into sleep, the toggling should stop. ''EDIT: is there any specific register in which we can select which peripherals can be clock gated'' For the SMT32F405 - yes. The registers are in the RCC register set. See the reference manual for details. ''or its jusy by enabling clock to peripherals'' Yes, you can manually control the peripherals. I have implemented both in my work because it give better power saving. I have turned off any peripheral that is not in use and only a small number of peripherals are clocked during Sleep mode, just the peripheral that may wake the processor.2014-05-23 3:54 AM
For clock gating , register in STM32F205RBT6 is RCC->AHB1ENR , depending upon peripheral.
Will enabling/disabling a particular register reinitialize all the peripheral register values. or it maintain the set values2014-05-23 4:20 AM
Hi
''For clock gating , register in STM32F205RBT6 is RCC->AHB1ENR , depending upon peripheral. Will enabling/disabling a particular register reinitialize all the peripheral register values. or it maintain the set values'' Please check the reference manual (possible data sheet) for definitive answer. I think that the peripheral(s) should remain unchanged when the clock is stopped and then restored.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.