2013-11-18 9:22 AM
I am a beginner with STM32F4 and I am study the ETH driver procedure but I don't understand some instructions
For example: /* Clear MBC bits in the selected MAC address high register */ (*(__IO uint32_t *) (ETH_MAC_ADDR_HBASE + MacAddr)) &=(~(uint32_t)ETH_MACA1HR_MBC); /* Wait until the write operation will be taken into account : at least four TX_CLK/RX_CLK clock cycles */ tmpreg = (*(__IO uint32_t *) (ETH_MAC_ADDR_HBASE + MacAddr)); _eth_delay_(ETH_REG_WRITE_DELAY); (*(__IO uint32_t *) (ETH_MAC_ADDR_HBASE + MacAddr)) = tmpreg; I don't understand the read and write same register after delay Thanks in advance for help #stm32f4-eth2013-11-18 9:37 AM
You'd need to find someone with a gate-level understanding of the design to talk to you, but the comments seem to suggest that there are consideration which fall under a different, slower, timing domain than the APB/AHB you are using to access the registers. ie pulling the bits off the wire, and checking the MAC address
2014-02-04 2:46 PM
It's a silicone bug workaround. See latest errata sheet ''2.7.5 Successive write operations to the same register might not be fully taken into account''.
2014-02-05 6:39 AM
Thanks, thanks a lot trushkin now is clear
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.