2023-05-31 3:03 AM
Hello dear friends,
does any one know how i can have 2 signal with 90 degree phase shift? but i want to use this easy bit pattern to have it and not pwm, just with this bit pattern 00, 01, 11, 10, and also a sleep time for delay, it shouldn't be difficult, i know that i just need one timer, for example TIM16, but i have no idea any more.
here are my codes and so i have 70 degree phase shift, do you have any idea?
Thank you
while (1)
{
HAL_TIM_Base_Start(&htim16);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, GPIO_PIN_RESET);
HAL_TIM_Base_Stop(&htim16);
HAL_TIM_Base_Start(&htim16);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, GPIO_PIN_SET);
HAL_TIM_Base_Stop(&htim16);
HAL_TIM_Base_Start(&htim16);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, GPIO_PIN_SET);
HAL_TIM_Base_Stop(&htim16);
HAL_TIM_Base_Start(&htim16);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, GPIO_PIN_RESET);
HAL_TIM_Base_Stop(&htim16);
static void MX_TIM16_Init(void)
{
/* USER CODE BEGIN TIM16_Init 0 */
/* USER CODE END TIM16_Init 0 */
/* USER CODE BEGIN TIM16_Init 1 */
/* USER CODE END TIM16_Init 1 */
htim16.Instance = TIM16;
htim16.Init.Prescaler = 8;
htim16.Init.CounterMode = TIM_COUNTERMODE_UP;
htim16.Init.Period = 1000;
htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim16.Init.RepetitionCounter = 0;
htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim16) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM16_Init 2 */
/* USER CODE END TIM16_Init 2 */
}
2023-05-31 3:26 AM
Period and Prescaler expect N-1 value
ie DIV8 is 7 (0..7 counts)
Phase shifted 50/50 duty quadrature, might consider Toggle Mode with different phase angles expressed via CCRx registers. Period = 399, CCR1 = 0, CCR2 = 100
2023-05-31 3:30 AM
i don't get it, i think i should use a counter maybe, but i don't know how!!! i am sure that i need just one Timer, but how i can generate these pulses i have no idea!!
2023-06-02 7:53 AM
i did it with interrupts, thanks freinds
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.