2019-01-10 2:50 AM
Hi Everyone!
I am using the STM32407IG and i am trying to send data to another mcu chip via USART RX TX Pins.
The Problem is when i run it via USB FS i don't get the baud rate adjusted.
How can i setup the Clock for a Baud rate of 9600?
That's my clock so far:
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 192;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 4;
HAL_RCC_OscConfig (&RCC_OscInitStruct);Here i have the baud rate in my code:
UartHandle.Instance = USARTx;
UartHandle.Init.BaudRate = 9600;
UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
UartHandle.Init.Mode = UART_MODE_TX_RX;
UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
Thanks for every help! :smiling_face_with_smiling_eyes:
Solved! Go to Solution.
2019-01-10 6:17 AM
I see you are using external clock. Please check if HSE_VALUE matches external clock frequency. By default, HSE_VALUE is set to 25000000, as I see from PLLM setting, you are using 8MHz clock, but this is just suspection.
2019-01-10 6:17 AM
I see you are using external clock. Please check if HSE_VALUE matches external clock frequency. By default, HSE_VALUE is set to 25000000, as I see from PLLM setting, you are using 8MHz clock, but this is just suspection.
2019-01-10 6:28 AM
Send an 0x55 pattern repetitively and scope the pin to check the bit-timing.
2019-01-10 6:47 AM
I used t a example cdc program
PLL_M = 25
PLL_N = 336
PLL_P = 2
PLL_Q = 7
that was the clock for default and i changed it because the vcp for USB FS doesn't connect with this clock
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.