2015-12-29 6:09 AM
My project contains a STM32F429 and a AS4C4M16S SDRAM (own designed PCB)
I have tested writing-reading by the next function:void SDRAM_TEST(void) {
int i; int err=0; int ok=0; HAL_StatusTypeDef ret; #define TEST_ARRAY_SIZE_WORD 10000 uint16_t x1[TEST_ARRAY_SIZE_WORD]; uint16_t x2[TEST_ARRAY_SIZE_WORD]; for (i=0; i<TEST_ARRAY_SIZE_WORD; i++) { //random data into the buffer x1[i]= rand(); } ret= HAL_SDRAM_Write_16b(&hsdram, SDRAM0, x1, TEST_ARRAY_SIZE_WORD); //write to SDRAM ret= HAL_SDRAM_Read_16b(&hsdram, SDRAM0, x2, TEST_ARRAY_SIZE_WORD); //reading SDRAM back into other buffer for (i=0; i<TEST_ARRAY_SIZE_WORD; i++) { if (x1[i] != x2[i]) err++; else ok++; //check if fits } } Surprisingly the ''err'' and ''ok'' values came out as 5000-5000! The debug values of x1 and x2 arrays are 0 f42d a01d 1 8ccf 8ccf 2 f646 f42d 3 3129 3129 4 5b04 f646 5 5db4 5db4 6 7f78 5b04 7 59d8 59d8 ... So even words are fine, odd words are shifted. It seems to be a word-order problem. Internally two 16-bit words are probably linked into one 32bit word, and the problem must be there somewhere... full code for FMC init is void MX_FMC_Init(void) { //********************************************** int i; HAL_StatusTypeDef ret; FMC_SDRAM_TimingTypeDef timing; hsdram.Instance = FMC_SDRAM_DEVICE; //Perform the SDRAM1 memory initialization sequence hsdram.Init.SDBank = FMC_SDRAM_BANK1; hsdram.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8; hsdram.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12; hsdram.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_16; hsdram.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4; hsdram.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_2; hsdram.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE; hsdram.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_3; hsdram.Init.ReadBurst = FMC_SDRAM_RBURST_DISABLE; hsdram.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0; //1?? //168MHz, tcycle= 11.9nsec timing.LoadToActiveDelay= 2; // TMRD: 2 Clock cycles timing.ExitSelfRefreshDelay= 7; //TXSR: min=65ns (6x11.9ns) timing.SelfRefreshTime= 5; //TRAS: min=49ns (5x11.90ns) timing.RowCycleDelay= 7; //TRC: min=63 nsec (6x11.90ns) timing.WriteRecoveryTime= 2; //TWR: 2 Clock cycles timing.RPDelay= 2; //TRP: min=21nsec (2x11.90ns) timing.RCDDelay= 2; //TRCD: min=21nsec (2x11.90ns ) ret= HAL_SDRAM_Init(&hsdram, &timing); //Initialize the SDRAM controller if(ret != HAL_OK) { i= 99; //bp here debug } SDRAM_Initialization_Sequence(&hsdram); //Program the SDRAM external device } void SDRAM_Initialization_Sequence(SDRAM_HandleTypeDef *hsdram) { //*********************************************** //static void SDRAM_Initialization_Sequence(SDRAM_HandleTypeDef *hsdram, FMC_SDRAM_CommandTypeDef *Cmd) { //*********************************************** FMC_SDRAM_CommandTypeDef Cmd; __IO uint32_t tmpmrd =0; Cmd.CommandMode= FMC_SDRAM_CMD_CLK_ENABLE; //Step 3: Configure a clock configuration enable command Cmd.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1; Cmd.AutoRefreshNumber= 1; Cmd.ModeRegisterDefinition= 0; HAL_SDRAM_SendCommand(hsdram, &Cmd, 0x1000); //Send the command HAL_Delay(100); //Step 4: Insert 100 ms delay Cmd.CommandMode= FMC_SDRAM_CMD_PALL; //Step 5: Configure a PALL (precharge all) command Cmd.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1; Cmd.AutoRefreshNumber= 1; Cmd.ModeRegisterDefinition= 0; HAL_SDRAM_SendCommand(hsdram, &Cmd, 0x1000); Cmd.CommandMode= FMC_SDRAM_CMD_AUTOREFRESH_MODE; //Step 6 : Configure a Auto-Refresh command Cmd.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1; Cmd.AutoRefreshNumber= 4; Cmd.ModeRegisterDefinition= 0; HAL_SDRAM_SendCommand(hsdram, &Cmd, 0x1000); tmpmrd = (uint32_t)SDRAM_MODEREG_BURST_LENGTH_2 | //Step 7: Program the external memory mode register SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL | SDRAM_MODEREG_CAS_LATENCY_3 | SDRAM_MODEREG_OPERATING_MODE_STANDARD | SDRAM_MODEREG_WRITEBURST_MODE_SINGLE; Cmd.CommandMode= FMC_SDRAM_CMD_LOAD_MODE; Cmd.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1; Cmd.AutoRefreshNumber= 1; Cmd.ModeRegisterDefinition= tmpmrd; HAL_SDRAM_SendCommand(hsdram, &Cmd, 0x1000); /* Step 8: Set the refresh rate counter 64msec / 4096 fresh = 15.62 us refresh count= 15.62usec * 84MHz - 20 = 1292 */ HAL_SDRAM_ProgramRefreshRate(hsdram, 1292); //refresh count }2015-11-22 9:55 AM
Hi, I'm facing a similar problem with same SDRAM. Can you publish the configuration that worked for you?
Thanks,2015-12-29 6:45 AM
> So even words are fine, odd words are shifted.
You mean, odd halfwords are fine, even are shifted. What is the result of direct reading, after the above test, e.g. if you add somevariable = *(uint16_t *)SDRAM0; someothervariable = *(uint32_t *)SDRAM0; after the above test, what are the x1[]/x2[]/somevariable/someothervariable? JW2015-12-30 11:47 AM
Thanks, Jan,
the FMC_SDRAM_CMD_LOAD_MODE command in SDRAM_Initialization_Sequence() was bad. I have simply copied the Mode parameters from some example code, which was for a different type of SDRAM...it was a miracle that even half of bytes fitted:))) I couldn't clearly understand how that happened... but now it's 10k/10k good!!! thanks, Tamas2017-02-03 8:44 AM
I'm a bit late, but here is the working source:
void SDRAM_Initialization_Sequence(SDRAM_HandleTypeDef *hsdram) { //***********************************************
//static void SDRAM_Initialization_Sequence(SDRAM_HandleTypeDef *hsdram, FMC_SDRAM_CommandTypeDef *Cmd) { //***********************************************FMC_SDRAM_CommandTypeDef Cmd;__IO uint32_t tmpmrd =0;Cmd.CommandMode= FMC_SDRAM_CMD_CLK_ENABLE; //Step 3: Configure a clock configuration enable commandCmd.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1;Cmd.AutoRefreshNumber= 1;Cmd.ModeRegisterDefinition= 0;HAL_SDRAM_SendCommand(hsdram, &Cmd, 0x1000); //Send the commandHAL_Delay(100); //Step 4: Insert 100 ms delayCmd.CommandMode= FMC_SDRAM_CMD_PALL; //Step 5: Configure a PALL (precharge all) command
Cmd.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1;Cmd.AutoRefreshNumber= 1;Cmd.ModeRegisterDefinition= 0;HAL_SDRAM_SendCommand(hsdram, &Cmd, 0x1000);Cmd.CommandMode= FMC_SDRAM_CMD_AUTOREFRESH_MODE; //Step 6 : Configure a Auto-Refresh command
Cmd.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1;Cmd.AutoRefreshNumber= 4;Cmd.ModeRegisterDefinition= 0;HAL_SDRAM_SendCommand(hsdram, &Cmd, 0x1000);tmpmrd = (uint32_t) //Step 7: Program the external memory mode register
0x0200 | //bit9: write burst length 1=single bit 0x0000 | //bit 8..7: test mode=0 normal mode 0x0020 | //bit 6..4: cas latency= 2 0x0000 | //bit 3: burst type=1 sequential 0x0000; //bit 2..0: burst length= 1 wordCmd.CommandMode= FMC_SDRAM_CMD_LOAD_MODE;Cmd.CommandTarget= FMC_SDRAM_CMD_TARGET_BANK1;Cmd.AutoRefreshNumber= 1;Cmd.ModeRegisterDefinition= tmpmrd;HAL_SDRAM_SendCommand(hsdram, &Cmd, 0x1000); /* Step 8: Set the refresh rate counter64msec / 4096 fresh = 15.62 us refresh count= 15.62usec * 84MHz - 20 = 1292 */HAL_SDRAM_ProgramRefreshRate(hsdram, 1292); //refresh count}2017-02-13 7:49 AM
Hi Thomas Novak
Ihave a custom made board around an STM32F429IIT6 connected to an external SDRAM AS4C4M16SA, I followed initialization steps embedded in the STM32F429 Reference Manual
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Freference_manual%2F3d%2F6d%2F5a%2F66%2Fb4%2F99%2F40%2Fd4%2FDM00031pdf%2Ffiles%2FDM00031pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.DM00031pdf
page 1663, and the Power Up sequence described in Note 11 of the AS4C4M16SA
/external-link.jspa?url=http%3A%2F%2Fwww.alliancememory.com%2Fpdf%2Fdram%2F64M-AS4C4M16SA.pdf
page
I configured also the same settings and initialization stepsthat you usedbutit fails for me.
Iused previously the MT48LC4M16 chip and it works fine, but the PCB design has changed and the old code doesn't fit the new AS4C4M16SA, the pins of the 2 chips are the same, and connections with the microcontroller are then the same.
Iuploaded my configuration files, my test functions, my serial_debug results and my schematic related to the memory power and pins.
Is there any difference inmy and your schematics ? Is there any problem with my code ?
I don't think that the problem is from a difference in the used libraries,CMSIS (for my case) and HAL
(for yours)arealmost the same especially for the SDRAM controller, and migrating toHAL library isn't a solution since I will be forcedto rewrite the wholeproject.
Thanks ________________ Attachments : Schematic and config Files.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyvn&d=%2Fa%2F0X0000000bE6%2FF0LAei5EkL4yZ8xgOI73RcJmHvXpUXtT7uosBBWwCbU&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.